sharring data between tasks using pipes in MQX 4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sharring data between tasks using pipes in MQX 4.2

1,418件の閲覧回数
ryanlush
Contributor IV

I am trying to share data between 2 tasks in MQX 4.2 using pipes. I am seeing data go in the pipe (and finally the task blocks when its full) but when I try to pull data out the other end there is nothing there. I have written a simple MQX 4.2 app that does just this and even it fails. Is there anything obvious I'm doing wrong? I have the pipes named differently in the two tasks but my understanding is that does not matter if they both open with the same "pipe1:" string.

#include <mqx.h>
#include <bsp.h>
#include <fio.h>
#include <io_pipe.h>

/* Task IDs */
#define HELLO_TASK 5
#define HELLO_TASK2 6

extern void hello_task(uint32_t);
extern void hello_task2(uint32_t);


const TASK_TEMPLATE_STRUCT  MQX_template_list[] =
{
    /* Task Index,   Function,   Stack,  Priority, Name,     Attributes,          Param, Time Slice */
    { HELLO_TASK,   hello_task, 1500,   8,        "hello",  MQX_AUTO_START_TASK, 0,     0 },
    { HELLO_TASK2,  hello_task2,1500,   8,        "hello2", MQX_TIME_SLICE_TASK, 0,     0 },
    { 0 }
};

static MQX_FILE_PTR inPipe1 = NULL;
static MQX_FILE_PTR outPipe1 = NULL;
static MQX_FILE_PTR inPipe2 = NULL;
static MQX_FILE_PTR outPipe2 = NULL;

/*TASK*-----------------------------------------------------
*
* Task Name    : hello_task
* Comments     :
*    This task prints " Hello World "
*
*END*-----------------------------------------------------*/
void hello_task
    (
        uint32_t initial_data
    )
{
    (void)initial_data; /* disable 'unused variable' warning */
    uint32_t nRead = 0;

    _io_pipe_install("pipe1:", 128, 0);
      
    inPipe1  = fopen("pipe1:",  "rw");

    _task_create(0, HELLO_TASK2, initial_data);

    while(1)
    {
        write(inPipe1, "FEEDBEEF", 8);
        
        ioctl(inPipe1, PIPE_IOCTL_NUM_CHARS_FULL, &nRead);

        _time_delay(1000);
    }

    
    _task_block();
}

void hello_task2
    (
        uint32_t initial_data
    )
{
    (void)initial_data; /* disable 'unused variable' warning */
    uint32_t nRead = 0;
    uint8_t buffer[128];
    
    inPipe2  = fopen("pipe1:",  "rw");

    while(1)
    {
        ioctl(inPipe2, PIPE_IOCTL_NUM_CHARS_FULL, &nRead);
            
        if (nRead > 0)
        {
            if (nRead > 128)
            {
                nRead = 128;
            }
            
            nRead = read(inPipe2, buffer, nRead);
        }

        _time_delay(50);
    }

    _task_block();
}

/* EOF */

0 件の賞賛
返信
1 返信

1,318件の閲覧回数
mjbcswitzerland
Specialist V

Ryan

I would try in the MQX forums for such questions:
https://community.nxp.com/community/mqx 
MQX RTOS Training 
MQX Downloads 


Although I don't think that MQX is supported by NXP any more. 

Regards

Mark

0 件の賞賛
返信