setting and initializing PDB at MCUXpresso Kinetis MKE1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

setting and initializing PDB at MCUXpresso Kinetis MKE1

1,424 Views
JohnEE
Contributor I

Hello there

when I try to set my PDB1 on MKE1 MCU at MCUXpresso .I can not set the triggered device to ADC1 !!

the only option to connect the PDB1 trigger output is to ADC0 !!?

how can I link PDB1 trigger signals to ADC1 ?

JohnEE_0-1610455031885.png

 

Tags (3)
0 Kudos
Reply
1 Reply

1,403 Views
nxf58904
NXP Employee
NXP Employee

Hi,

You can modify the code directly to trigger adc1 via pdb1.The main areas need to be modified has been marked in red.

I will update if here has some issue.

nxf58904_0-1610679892234.png

 

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply