second request - - need the schematic symbol for the KV5 series - - - would like both the 100 pin and 144 pin package schematic symbol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

second request - - need the schematic symbol for the KV5 series - - - would like both the 100 pin and 144 pin package schematic symbol

1,976 Views
jamespottebaum
Contributor I

would like both the 100 pin and 144 pin (none BGA)   that is schematic symbol and not the PCB layout for the package - - -

I know freescale has to have this somewhere for they have laid out boards and I am sure used the schematic symbol

thanks

Jim P

Labels (1)
0 Kudos
Reply
3 Replies

1,806 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi James Pottebaum

Please refer to the next link:

Kinetis CAD Schematics, Symbols & Footprints|NXP 

Hope this help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,806 Views
jamespottebaum
Contributor I

this is my third request - - - Ultra lib does not have enough

information -- - - can you stop and hear what I am saying - - -

it never has - - - - I need the schematic symbol with the Alt functions

listed - - - from what I understand the free version does not allow me

to see if it has been improved - - but sample part shows it has not been

-- -- - - -

0 Kudos
Reply

1,806 Views
jamespottebaum
Contributor I

every time that I have used Ultalib - - - It did not have what I needed

- - - sure the square box - - pins numbered and on function just the

port pin name and no alt functions - - - - so was totally a waste of

time to try to use it.

now in your system you have laid out boards - you have done schematics

- - - I need what you used internally

every time I have needed the schematic symbol - - I have this dam debate

with Freescale/NXP - - - and I am getting tried of it.

Jim P

0 Kudos
Reply