sdhc_drv_init() fail?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdhc_drv_init() fail?

5,657 Views
audi_mcavoy
Contributor IV

My 2GB Transcan microSD card does not initialize correctly when my FRD-K64F is powered up.  Only after pressing the reset button is the card accessible.  Well, almost "only."

 

Using KDS, I have created a simple app based on the FRDM-K64F with PE and KSDK support.

 

Using PE, I added a debug console (debug_console), a memory card (fsl_sdcard) and a GPIO pin (fsl_gpio) to my project.  The memory card is setup for 4-bit access, and the GPIO pin is setup as a card detect input.  Everything is configured from the FRDM-K64F schematic.

 

On power up, the blocksize member in my sdhc_card_t structure is "0" (in fact, all members appear to be zeroed), and the card is not accessible.  Pressing the reset button then initializes the card structure, and everything works as expected.

 

I have also found that shutting down the SDHC driver, then reinitializing the SDHC and the SDCARD drivers "fixes" the problem.  Like this. . .

 

if (0 == memoryCard1_state.blockSize) { #if 0   SDCARD_DRV_Shutdown(&memoryCard1_state); #endif    SDHC_DRV_Shutdown(FSL_FSL_SDHC1);    if (kStatus_SDHC_NoError != SDHC_DRV_Init(FSL_FSL_SDHC1, &fsl_sdhc1_host, &fsl_sdhc1_InitConfig0)) {     printf("SDHC_DRV_Init() error\r\n");     return false;   }    if (kStatus_SDHC_NoError != SDCARD_DRV_Init(&fsl_sdhc1_host, &memoryCard1_state)) {     printf("SDCARD_DRV_Init() error\r\n");     return false;   }    if (0 == memoryCard1_state.blockSize) return false; } return true;

 

Notice that calling SDCARD_DRV_Shutdown() hung the processor.  On the other hand, not calling SDHC_DRV_Shutdown() followed by SDHC_DRV_Init() was not sufficient to restore SD card access.  Also, calling SDHC_DRV_Init() without first calling SDHC_DRV_Shutdown() was problematic.

 

I've attached my project.

 

Does anyone have any suggestions?

Original Attachment has been moved to: sdcard_test.zip

Tags (3)
0 Kudos
Reply
10 Replies

5,214 Views
audi_mcavoy
Contributor IV

I was pulled away from this project for a while, but I'm back on it now.

Since my original post, I have attended FTF 2015, switched from KDS 2.0 to KDS 3.0, and switched from KSDK 1.1 to KSDK 1.2.  I built a new project hoping the bug was fixed, but it's still there.

My original post implied that the problem only appeared when the board was first "powered up."  I have done a lot more investigating since, and I don't believe that's a true statement.  I do believe the problem presents itself when the code is launched with the OpenSDA debugger.  Every time I launch the program with the debugger, the SD card driver fails to initialize.  It returns an error code 3, which fsl_sdhc_driver.h enumerates as kStatus_SDHC_SetCardToIdle  /*!< Failed to set card to idle */

If I then hit the reset button, it works.  If I power cycle the board, it works.

The only way I can get it to work with the debugger is to shutdown the SDHC driver, reinitialize it and then reinitialize the SDCARD driver (as shown in the original post).

- Audi

0 Kudos
Reply

5,214 Views
BlackNight
NXP Employee
NXP Employee

In case this is relevant:

I faced several problems with SD cards and power consumption of them on the FRDM-K64F board: some SD-cards drain several hundreds of milli-Amps when inserted or powered up. And the 5V to 3.3V DC-DC converter was not able to power all the devices on the board (K20, K64F plus the SD card).

So is this problem only happening if you have the SD card inserted at power-up time?

Our solution was to use industrial grade SD cards which had a much better (lower) power-up current consumption.

Or you might backup the 3.3V on the header with some more milli-amps. You might be able to measure a power drop on the 3.3V too.

I hope this might be useful,

Erich

0 Kudos
Reply

5,214 Views
giacomopetrini
Contributor IV

Have you solved?

I found out that some SDCards need some time to "wakeup" when first powered, so in my project I wait 1 second before trying to initialize the SDHC driver, and it always work.

If I don't wait, depending on the sdcard sometime it work, sometime I have the same behaviour as you.

Best Regards

Giacomo

0 Kudos
Reply

5,214 Views
audi_mcavoy
Contributor IV

Giacomo, I have not found a solution.

I have also noticed that some SD cards need a few seconds to "wake up."  I did try putting in some different delays in different locations; but, nothing made a difference.

Thanks for the suggestion though.

- Audi

0 Kudos
Reply

5,214 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Audi,

I have test your project on my side , and it can work well , the screenshot below is the information on hyperterminal.

pastedImage_0.png

Does i misunderstand your question ?

BR

Alice

0 Kudos
Reply

5,214 Views
audi_mcavoy
Contributor IV

Hi Alice,

Did you get it to work from KDS with the OpenSDA debugger?  Or did you drag/drop onto the mbed drive?

0 Kudos
Reply

5,214 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Audi ,

I recommend you test the SD demo under KSDK (...\KSDK_1.1.0\demos\sdhc_sdcard) .

BR

Alice

0 Kudos
Reply

5,214 Views
audi_mcavoy
Contributor IV

Yep.  Did that first.

Most of my (SD) code was copy/paste from there.

- am

0 Kudos
Reply

5,215 Views
mjbcswitzerland
Specialist V

Hi

See whether you get the same behaviour with a FRDM-K64F binary from: µTasker Kinetis FRDM-K64F support

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply

5,214 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I moved your thread to the correct place.

Regards

Vicente

0 Kudos
Reply