s9keaz128a MLH reset pin problem,MCU can not boot properly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s9keaz128a MLH reset pin problem,MCU can not boot properly

跳至解决方案
2,115 次查看
lynger
Contributor I

Hi all,

I'm using s9keaz128a MLH 2N45K CTHE 1811G for a automotive project as a motor controller. However the board doesnot running properly as expected. It could not boot. The 5V VCC is OK with no noise, But the #s9keaz128a Reset pin (without capacitor) is poor like this:

poor_s9keaz128a_boot1.jpg

and with capacitor ( 2.3V plus Sawtooth Wave noise):

poor_s9keaz128a_boot2.jpg

the reset pin(pa5/reset_b 63 pin) circuit:

pastedImage_3.png

the reset should be 5V. 

标记 (2)
0 项奖励
回复
1 解答
1,927 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Lynger Zhu,

Please refer: How To Sucessfully Program a Custom made Kinetis Microcontroller Board.
Notice the circuit of these pins:

NMI_b          external pullup resistor

SWD_CLK   external pulldown resistor

SWD_DIO   external pullup resistor


You can attach your circuit here, so that we can check it.

If still not work, please try to use 3.7uF Vdd bypass capacitor.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,927 次查看
lynger
Contributor I

Problem solved.

It's caused by the NMI_b.The board's NMI_b pin was used as a gpio and connect to a BJT with a pulldown resistor.So the fresh new MCU was interrupted again and again. The MCU never boot properly not to mention flash firmware.

We will change the board gpio next time.

0 项奖励
回复
1,928 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Lynger Zhu,

Please refer: How To Sucessfully Program a Custom made Kinetis Microcontroller Board.
Notice the circuit of these pins:

NMI_b          external pullup resistor

SWD_CLK   external pulldown resistor

SWD_DIO   external pullup resistor


You can attach your circuit here, so that we can check it.

If still not work, please try to use 3.7uF Vdd bypass capacitor.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------