recommendation automotive CAN eval board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

recommendation automotive CAN eval board

3,347件の閲覧回数
momo12
Contributor III

Hi

for a concept car I need to drive a SPI based LED strip (ws2812) . In this project RGB information to drive the LEDs will be received via can protocol. So input from CAN output VIA SPI.

I have some s32k experience, but S32K is too expensive and seems to be an overdrive for this project. Then I thought of a Kinetis, but Kinetis is not on the list of my customers (major car brand) allowed processors(S32k is on the list).

Does NXP have a different processor in his portfolio which is cheaper?

Is Kinetis already outdated?

Actually I dont see Kinetis on vector's list of processors eithers! Whsy is that?

https://vector.com/portal/medien/cmc/datasheets/CANbedded_Availability_EN.pdf 

Thx

0 件の賞賛
返信
1 返信

3,052件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Well, for the Automotive application, besides the S32K, we really has much chip family resource to support it, for example S08,S12 and MPC5. I am attaching here a quite useful document for your reference/selection.

0 件の賞賛
返信