pwm using dma transfer datas to cnv

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pwm using dma transfer datas to cnv

Jump to solution
2,367 Views
fugrace
Contributor III

hi everyone ,I have this problem for several days and still no solution.

I want to send data to the PWM module's C0V register to change its duty cycle by enable the DMA.

But I really don't know what's wrong with my code .It seems that the DMA transmission is failed because the value of C0V  is always 0.

I have succeed in generating pwm by updating the C0V through the MPU,like below:

while(1)

{

  FTM0_C0V = pwm1;

  FTM0_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK;

}

and I've also succeed in transfering datas from memory to memory by using DMA.But it never works when I connect the DMA to PWM register.

By the way ,I'm using the DMA in periodic trigger mode,and I think I have configured the PIT module right.

My code are as follows:

//dma.c

/***channel init***/

void DMAinit(int chno,int sourceno)

{

     SIM_SCGC6 |= SIM_SCGC6_DMAMUX_MASK;

     DMA_SERQ|=DMA_SERQ_SERQ(chno) ;//enable the source  chno

     DMAMUX_CHCFG(chno)=(DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(sourceno));//enable dma channel chno,

     DMAMUX_CHCFG(chno)|=DMAMUX_CHCFG_TRIG_MASK;//enable the periodic trigger

}

//DMA controler setting

void DMAset(uint32 *source_addr,uint32 *destiny_address,char sbits,char dbits,char nbytes,char chno,uint16 majorinter )

{

  uint8 i;

  i =chno ;//DMA  number of channel

  SIM_SCGC7 |= SIM_SCGC7_DMA_MASK; //enable DMA clock

  DMA_SADDR(i) = (uint32)source_addr;//DMA source address

  DMA_DADDR(i) = (uint32)destiny_address;//DMA destiny address

  DMA_NBYTES_MLNO(i)  =2;//minor loop  nbytes

  DMA_ATTR(i)= (DMA_ATTR_SSIZE(sbits)|DMA_ATTR_DSIZE(dbits)) ;//source and dest bits 

  DMA_SOFF(i) =0x2; //source address offset after each transfer

  DMA_DOFF(i)=0x0;/source address offset after each transfer

  DMA_SLAST(i) = -nbytes;   //adjust the source address to the original address

  DMA_DLAST_SGA(i) = -nbytes;    /adjust the destiny address to the original address

  DMA_CITER_ELINKNO(i) =DMA_CITER_ELINKNO_CITER( majorinter);//current major loop counts

  DMA_BITER_ELINKNO(i) = DMA_BITER_ELINKNO_BITER(majorinter);//beginning major loop counts

  DMA_CSR(i)|=DMA_CSR_BWC(3);//bandwidth control

  //DMA_CSR(i)|=DMA_CSR_INTMAJOR_MASK;

  DMA_CSR(i)|=DMA_CSR_START_MASK;//soft start

  //DMA_SERQ|=DMA_SERQ_SERQ(chno) ;//enable hardware request  chno (have done in the DMAinit)

}

//main.c

int main(void)

{

    InitPWM();

    hw_pit_init(PIT1,0x249f00);//set the timeout of PIT1

    DMAinit(1,ftm0ch0_dmasc);//

    DMAset(pwmdata,(uint32)&FTM0_C0V,1,1,buflength*2,1,30);

    while(1);

  return 0;

}

Labels (1)
0 Kudos
Reply
1 Solution
2,044 Views
fugrace
Contributor III

Hi,Paul

Thanks so much for checking my code so carefully.But I really have to say sorry .Because when I restart my job today(and that's why I reply late.) I finally found there's no problem with my code,it's just because the DMA transfer is so fast that I can only see the finally result : 0,and that's the same value when the CnV begins.When I changed the value ,I can see the right result now. And now I'm working on how to slow down the DMA.

Grace

View solution in original post

0 Kudos
Reply
7 Replies
2,044 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Grace

I checked your code. I think I need to confirm something with you. As you mentioned, it seems that you tested two DMA function. One is FTM0 channel0 and the other is PIT. In your first testing, I cannot find FTM0 channel0 intial code. So please make sure that you enable DMA function in your FTM control register. For example, you need to set bit DMA in FTM0_C0SC.

In your second PIT testing, I find that your ciode seems still use FTM0 channel0 in your DMA setting. If my understanding on your testing is incorrect, please correct me.

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply
2,045 Views
fugrace
Contributor III

Hi,Paul

Thanks so much for checking my code so carefully.But I really have to say sorry .Because when I restart my job today(and that's why I reply late.) I finally found there's no problem with my code,it's just because the DMA transfer is so fast that I can only see the finally result : 0,and that's the same value when the CnV begins.When I changed the value ,I can see the right result now. And now I'm working on how to slow down the DMA.

Grace

0 Kudos
Reply
2,044 Views
rastislav_pavlanin
NXP Employee
NXP Employee

Hi,

it is looking like you are faceing an errata. It is not clear what device with what silicon mask you are using. Therefore, please check silicon mask errata for the device you are using. Or just simply try to trigger DMA request by another source (another FTM module etc.).

0 Kudos
Reply
2,044 Views
fugrace
Contributor III

Thank you ,I'm using K10,but I don't know what you mean by 'errata',I can't find it.Can you give me more direction?

0 Kudos
Reply
2,044 Views
rastislav_pavlanin
NXP Employee
NXP Employee

Hi,

errata in general is a document which inludes description of all bugs (not correctly working parts) of device. In Kinetis case it describes all bugs for specified silicon mask. You can find the silicon mask on the chip directly under device name MK10.... (e.g. 2N22 can be silicin mask). After visit our freescale sites and search for kinetis K10 errata.

For example here you can find something:

Freescale Search

0 Kudos
Reply
2,044 Views
fugrace
Contributor III

Hi,Thank you so much that now I really find your suggestion lead me to the finally result!

It is an errta

e4588: DMAMUX: When using PIT with "always enabled" request, DMA request does

not deassert correctly.

anyway,after many efforts I solved the PIT problem.now it works with DMA.

but still I have another problem, I guess you can give me a hand again. The DMA destination value doesn't

change although it enters into the DMA interrupt at the first three times.later it works well .then it drops the first three values

I want to send. Any suggestion?

Thank you again.

0 Kudos
Reply
2,044 Views
fugrace
Contributor III

Thank you ,it's useful for my later work.Though now I've checked it's not the problem of my code.

0 Kudos
Reply