project creation using IAR for MKE02Z64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

project creation using IAR for MKE02Z64

1,713件の閲覧回数
saravananselvam
Contributor I

hello everyone,

I'm new to Freescale MKE02Z64, can anyone help me in creating a project for this kind of processor using IAR Workbench and i've searching for past one week but couldnt find any tutorial for this kind of processor.

Thanks in advance...

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,486件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi saravanan,

Please download the 'FRDM-KEXX Driver Library Package (REV 1.2.1)' first.

And then you can find the 'make_new_project_ke02.exe' in it's folder(C:\KEXX_DRIVERS_V1.2.1_DEVD\kexx_drv_lib\build\iar\ke02).

make_new_project_ke02.png

Simply double-click make_new_project_ke02.exe file and a command prompt pop-up window will prompt you for a project name, copy the platinum project and rename all of the necessary files for your new project to work correctly.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,486件の閲覧回数
mjbcswitzerland
Specialist V

Hi Saravanan

There is an IAR project for your device in the Open Source uTasker prject at the links below. You just need to open \Applications\uTaskerV1.4\IAR7_Kinetis\uTaskerV1.4.eww for a complete application solution and \Applications\uTaskerSerialBoot\IAR7_Kinetis\uTaskerSerialBoot.eww for a complete serial loader solution.
Follow the IAR guide at http://www.utasker.com/kinetis/compilers.html#IAR if needed.

Regards

Mark

Code: http://www.utasker.com/kinetis.html
Board references:
- http://www.utasker.com/kinetis/FRDM-KE02Z.html
- http://www.utasker.com/kinetis/FRDM-KE02Z40M.html

0 件の賞賛
返信