Hi,
MCUBOOT is not available for MK21FN as SDK middleware but I wonder if I can get this package for the MK22FN (in this case yes, it's available) and port it to the MK21FN MCU. How difficult would it be?
Thanks in advance,
GS
Solved! Go to Solution.
 
					
				
		
 jingpan
		
			jingpan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @gschelotto ,
I think it wouldn't be very difficult. MK21FN architecture is similar to K22F120M. K21FN has SDK too. So,
1. use the K21FN SDK toreplace the driver and chip related file.
2. IO configuration.
3. maybe some clock
4. The peripherals which is used for download applications.
Regards,
Jing
 
					
				
		
Hi Jing,
I've finally ported the MCU boot to my custom MK21 board following your suggestions. Everything work as expected and it's totally compatible with our CAN tools used for the MK22 ROM Bootloader. Thank you for the given support!
regards,
gaston
 
					
				
		
 jingpan
		
			jingpan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @gschelotto ,
I think it wouldn't be very difficult. MK21FN architecture is similar to K22F120M. K21FN has SDK too. So,
1. use the K21FN SDK toreplace the driver and chip related file.
2. IO configuration.
3. maybe some clock
4. The peripherals which is used for download applications.
Regards,
Jing