plc G-3 modem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

plc G-3 modem

1,365 Views
mariuszslonina
Contributor II

Hi all. Where I can found more information about this solution ?

https://www.nxp.com/docs/en/reference-manual/DRM170.pdf 

Tags (1)
0 Kudos
Reply
1 Reply

1,277 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Mariusz,

That solution was a third party design so we don't have the source code of the application. Maybe you can ask them directly and see if they have available either SW or HW.


http://www.andrea.fr/

Sorry for the inconvenience this may cause you.

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply