osMutexDelete / osSemaphoreDelete result in a HardFault at "SVC 0".

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

osMutexDelete / osSemaphoreDelete result in a HardFault at "SVC 0".

跳至解决方案
1,160 次查看
omidontop
Contributor I

Greetings!

I'm running the Texas Instruments SimpleLink driver ( for CC3100 ) which I have ported to the mbed platform on a FRDM-K64F board with a MK64FN1M0VLL12 ARM Cortex-M4F processor. Now at some point the driver which I'm running from my main() function tries to delete the Semaphores and Mutexes which it previously allocated. the problem is that this simple operation results in a HardFault. Now I am certain that these Mutexes and Sepmaphores are actually allocated.

I have stepped through the instructions and I can see that "svc 0" is where the HardFault is triggered.

xhardfault.jpg.pagespeed.ic.b_nxVSTMmZ.webp

Does anyone have any clues as to why this might be happening?? I would appreciate any help.

标记 (2)
0 项奖励
回复
1 解答
1,021 次查看
omidontop
Contributor I

OK, I found the problem! The issue was that the code I was using called a __disable_irq() right before those instructions which I reckon resulted in HardFault exception!

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,022 次查看
omidontop
Contributor I

OK, I found the problem! The issue was that the code I was using called a __disable_irq() right before those instructions which I reckon resulted in HardFault exception!

0 项奖励
回复