openSDA for Mac OS X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

openSDA for Mac OS X

2,596 次查看
tamermash
Contributor II

Hello,

Will openSDA be available for Mac? I have KDS installed and configured to use openSDA; only thing I'm missing now is the openSDA binaries for Mac so the port gets created and I can use it.

I tried to manually build openSDA2 from its sources; however, it's setup to use the the Keil IDE, which is not free and I only saw a Windows version of it.

Is support for that coming? Or is it already here and I can't find it?

Thanks,

Tamer

标签 (1)
标记 (2)
2 回复数

1,484 次查看
BlackNight
NXP Employee
NXP Employee

Hi Tamer,

keep in mind that not all devices are supported in OpenSDA.

But there is a OpenSDA binary build available for Mac OS X here: The GNU ARM Eclipse OpenOCD | GNU ARM Eclipse

I have not tried it myself, but I expect that this one will work for you.

I hope this helps,

Erich

0 项奖励
回复

1,484 次查看
tamermash
Contributor II

Hi Erich,

The hardware that I have uses OpenSDA for debugging. It's a dev board and has that built-in. I will probably get a j-link for the real board, but I need to get it going with the dev board first.

Thanks and best regards,

Tamer

0 项奖励
回复