openSDA for Mac OS X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

openSDA for Mac OS X

3,439件の閲覧回数
tamermash
Contributor II

Hello,

Will openSDA be available for Mac? I have KDS installed and configured to use openSDA; only thing I'm missing now is the openSDA binaries for Mac so the port gets created and I can use it.

I tried to manually build openSDA2 from its sources; however, it's setup to use the the Keil IDE, which is not free and I only saw a Windows version of it.

Is support for that coming? Or is it already here and I can't find it?

Thanks,

Tamer

ラベル(1)
タグ(2)
2 返答(返信)

2,327件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Tamer,

keep in mind that not all devices are supported in OpenSDA.

But there is a OpenSDA binary build available for Mac OS X here: The GNU ARM Eclipse OpenOCD | GNU ARM Eclipse

I have not tried it myself, but I expect that this one will work for you.

I hope this helps,

Erich

0 件の賞賛
返信

2,327件の閲覧回数
tamermash
Contributor II

Hi Erich,

The hardware that I have uses OpenSDA for debugging. It's a dev board and has that built-in. I will probably get a j-link for the real board, but I need to get it going with the dev board first.

Thanks and best regards,

Tamer

0 件の賞賛
返信