open SDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,705件の閲覧回数
nesrinemhiri
Contributor III

Hello,

I have a FRDM-KL46Z kit,I use Embeded IAR,my problem that i can't connect to my device:untitled3.bmpss.bmpaa.bmp

1 解決策
5,366件の閲覧回数
nesrinemhiri
Contributor III

Hi

yes Iva the problem is in the USB drivers but i show the Article and i dont find any thing that can help me :smileysad:.

Regards,

Nesrine

untitled.bmp

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,366件の閲覧回数
gblack
Contributor I

Make sure you have the latest OpenSDA firmware installed. Also try uninstalling and reinstalling the driver from P&E Microcomputer Systems

0 件の賞賛
返信
5,366件の閲覧回数
nesrinemhiri
Contributor III

Hi

yes Iva the problem is in the USB drivers but i show the Article and i dont find any thing that can help me :smileysad:.

Regards,

Nesrine

untitled.bmp

0 件の賞賛
返信
5,366件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi nesrine mhiri,

please, check if you see it in your Computer.

computer.png

If yes, look into the storage. There is info.htm and you see in the file information about versions.

It looks that you have not installed PEMicro OpenSDA Debug Driver.

You may to install new software from PEmicro sites. Please, look here

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse

I hope it helps,

Iva

5,366件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi nesrine mhiri,


It looks like problem with fixing usb drivers.

please, check jungo driver. Our colleague created great article about it. http://mcuoneclipse.com/2012/10/12/fixing-the-usb-drivers/


I hope it helps,

Iva

0 件の賞賛
返信
5,366件の閲覧回数
omolin
Contributor II

Make sure you have loaded the Pemicro debug application in OpenSDA.

There is no way to tell if you have done this because you don't show the Pemicro device in device manager. The Serial port there is a general OpenSDA device so you could have no debug application loaded, or have CMSIS-DAP loaded possibly.

5,366件の閲覧回数
nesrinemhiri
Contributor III

really i don't find the problem,when i work with tower i usally use the JTAG pins but with FRDM kits am obliged to use the SDA ,please help me to connect to my kit

untitled.bmp