mqx for kinetis k20

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mqx for kinetis k20

1,364 Views
gagangarg
Contributor II

hello,

I am currently working on a project, where  I have to handle several real time data. I am using k20 to achieve the target.

I am getting in dealing with all these interrupts. So thought to implement mqx rtos in the project.

Can anyone suggest me whether it is feasible to use mqx with k20.

In the project i am dealing with these peripherals:

-dma

-gpio

-can

-usb-otg

-serial

Thank you,

Gagan Garg

0 Kudos
Reply
1 Reply

1,189 Views
dspNeil
Contributor III

Yes, MQX would work well for you in this scenario running on a K20. More importantly, which version of the K20 are you running? The silicon version (50MHz, 72MHz, 100MHz, etc...) is more important for starting your MQX port than is the K20 designation. A K20 100 MHz part is more closely related to a K40 100 MHz part than it is to a K20 50 MHz part. The "20" is more telling of the peripheral set of the part than it is of the silicon.

0 Kudos
Reply