mpc5744 Adc sampling inaccurate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc5744 Adc sampling inaccurate

1,410件の閲覧回数
chenbg188175751
Contributor I

MPC5744P chip ADC sampling, the reference voltage is 5V ,ADC0 and ADC1 sampling port peripheral reference voltage circuits are the same. The software is configured with ADC0 port 0 channel, ADC1 port 0 channel sampling at the same time, the external input analog voltage has 0 ~ 5 V change; Phenomenon: ADC0 port 0 channel sampling is normal, external voltage 2.5 V shows AD value 2045; When the external voltage of the ADC1 port 1 channel is 2.5V, the AD value 1750A DC0 changes linearly with the external voltage analog signal, and the ADC1 changes linearly with the external voltage analog signal (0 v corresponding to AD value 0 V to 5 v to AD value 4095, intermediate nonlinearity).

May I ask which points may have caused this phenomenon to occur?

0 件の賞賛
返信
1 返信

1,253件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Do you use our EVB for these tests or its your own custom board?

Do you calibrate ADCs before conversion?

Did you tried to measure it on different pins for ADC1?

regards,

Peter

0 件の賞賛
返信