mkv46f256 FLEXPWM module fault protection register question!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mkv46f256 FLEXPWM module fault protection register question!

1,304件の閲覧回数
jeffzxg
Contributor I

hello

      KV4XP100M168 Reference manual  say that:  flexpwm module has fault channel0 无标题.png,  but

in this module , it has PWMA_SMnDISMAP0 and PWMA_SMnDISMAP1  two dismap registers.  PWMA_SMnDISMAP0 controls fault channel0 and PWMA_SMnDISMAP1 controls fault channel1.  but fig37-1 say this module only has fault channel0 ,  does this mean PWMA_SMnDISMAP1  register has no use? only PWMA_SMnDISMAP0 work.  thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,183件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

After I've had look through the KV4x and KV5x reference manual, I think there's the document error, the PWMA_SMnDISMAP1 is invalid.

So I'd like to suggest that you can just ignore it.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信