mkv31f128 bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mkv31f128 bootloader

3,094件の閲覧回数
senthilprabhug
Contributor I

now i currently working with MKV31F128VLH10 microcontroller. I want add bootloader for field upgrade able. But i struggle with to create the bootloader code. I also sdk example for this controller but there is no sdk example for this controller. Please guide me how to create the bootloader code for this controller.

Have a great day,

Senthilprabhu.G

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,861件の閲覧回数
oscarniño
Contributor III

Hi Senthilprabhu G

Sorry did you get the bootloader, I'm starting to work with this MCU but I have the same problem. I have check examples downloading SDK with SDK builder but there is no examples for MKV31F128xxx10. Just for MKV31F512xxx12. Could you help me? If you can't share your code, cold you guide me in how to get it? Right now I need to know If has to set an especific configuration of pins for the PCB design to get a bootloader by I2C and UART. Thanks a lot:

Best Regards

0 件の賞賛
返信

2,861件の閲覧回数
senthilprabhug
Contributor I

Hi Oscar Nino,

   There is no example code for MKV31F129xx10. Use MKV31F512xxxx to get the example codes. But there is also no example codes for Bootloader. There is no any specific pins for for bootloader. You can use normal uart pins or I2C pins for bootloader.

Have you ever tried with the Kinetis Bootloader which you can download from the link below:

https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0

And here is the document for detail operation:

https://www.nxp.com/docs/en/user-guide/MBOOTFLASHGS.pdf 

Best Regards

0 件の賞賛
返信

2,861件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Have you ever tried with the Kinetis Bootloader which you can download from the link below:

https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0

And here is the document for detail operation:

https://www.nxp.com/docs/en/user-guide/MBOOTFLASHGS.pdf 

0 件の賞賛
返信

2,861件の閲覧回数
mjbcswitzerland
Specialist V

Hi Senthilprabhu

Various boot loaders are readily available for immediate use on the KV31F - see
- http://www.utasker.com/kinetis/FRDM-KV31F.html
- http://www.utasker.com/kinetis/TWR-KV31F120M.html

These are proven and documented: Serial Loader: http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf
and can be build/customised with MCUXpresso, KDS, S32 Design Studio, CW 10.x, IAR, Keil, CooCox, Green Hills, Rowley Crossworks, Atollic, GCC make file or VisualStudio.

Regards

Mark

0 件の賞賛
返信