mkl16xx and audio codec interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mkl16xx and audio codec interface

1,302 次查看
tuananhnguyen
Contributor I

hi all !

i'm new in kinetis

i'm using MKL16Z128VFM4 to communicate witch max9860 codec

the codec has mclk,lrclk,bclk,sdin,sdout pins

and the mcu has I2S0_TXD0,I2S0_TX_FS,I2S0_TX_BCLK,I2S0_MCLK,I2S0_RXD0,I2S0_RX_BCLK,I2S0_RX_FS

could you show me how to connect these pins

thanks!

标签 (1)
0 项奖励
回复
1 回复

1,215 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello tuan,

For i have not fund the reference manual , so i don't know the pin lrclk mean, you can check or you can send it to me .

About the other pins i guess as this below  , you can refer to :

kl16      -----            MAX9860

I2S0_MCLK            mclk

I2S0_TX_BCLK      bclk

I2S0——TXD0        sdin

I2S0_RXD0            sdout

I2S0_SDA              sda

i2s0_SCL              scl

I recommend you read the RM check all of the meaning of pins .

Hope it helps!


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复