mk64FN1M0VLL12 F/W download question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mk64FN1M0VLL12 F/W download question

1,237件の閲覧回数
hokinsliu
Contributor I

Hi ,

There is a question about flashing the f/w of K64F's IC,
when I finish to develop my mbed OS project, then I want to shrink the size of prototype, so i want to prepare a MK64FN1M0VLL12 IC and mount into my new prototype, it's a new layout PCB, and not using FRDM-K64F develop platform.

so, it comes to a question: How can I download the mbed OS F/W into the new prototype?
I am trying to using Kinetis IDE, it looks like the project needs to create a project then program it by using IDE, then I change to using keil uvision5 with Ulink2, it looks like the same as Kinetis like.

is anyone know how to solve this question?

0 件の賞賛
返信
1 返信

1,015件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Hokins,

How did you use to flash the firmware to your previous prototype?

You can use an external programmer like a P&E Multilink or Segger J-link to program the MCU trough the SWD/JTAG connector.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信