mk22fn512vll12 replacement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mk22fn512vll12 replacement

1,920件の閲覧回数
martindusek
Contributor V

Hello,

I have hard time finding direct replacement for mk22fn512vll12 (all major distributors are out of stock). I need same package, 16-bit flexbus, 3x FTM on the same pins.

Can you please advise replacement or where to buy?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,747件の閲覧回数
martindusek
Contributor V

I found MK22FN1M0VLL12. From reference manual I can't find any difference (at least pinout seems to be same as mk22fn512vll12).

0 件の賞賛
返信

1,747件の閲覧回数
troelsoesteraa
Contributor III

If you do not need USB for anything, and you can make a few changes to your schematic, I believe MKV31F512VLL12 would be a good, and nearly pin-compatible solution. I did not check it in detail, so be very careful!

0 件の賞賛
返信

1,747件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

The status for part mk22fn512vll12 is active and there has no "replacement" we can recommend. For the availability, yes, I know that there really become an issue recently. Anyway, please make reference from this post (https://community.nxp.com/docs/DOC-340645 )and I am pretty sure that the stock will recover soon.

0 件の賞賛
返信