mk22fn512vll12 replacement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mk22fn512vll12 replacement

1,942 Views
martindusek
Contributor V

Hello,

I have hard time finding direct replacement for mk22fn512vll12 (all major distributors are out of stock). I need same package, 16-bit flexbus, 3x FTM on the same pins.

Can you please advise replacement or where to buy?

Labels (1)
0 Kudos
Reply
3 Replies

1,769 Views
martindusek
Contributor V

I found MK22FN1M0VLL12. From reference manual I can't find any difference (at least pinout seems to be same as mk22fn512vll12).

0 Kudos
Reply

1,769 Views
troelsoesteraa
Contributor III

If you do not need USB for anything, and you can make a few changes to your schematic, I believe MKV31F512VLL12 would be a good, and nearly pin-compatible solution. I did not check it in detail, so be very careful!

0 Kudos
Reply

1,769 Views
miduo
NXP Employee
NXP Employee

Hi,

The status for part mk22fn512vll12 is active and there has no "replacement" we can recommend. For the availability, yes, I know that there really become an issue recently. Anyway, please make reference from this post (https://community.nxp.com/docs/DOC-340645 )and I am pretty sure that the stock will recover soon.

0 Kudos
Reply