mk22fn1m0vlk12 bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mk22fn1m0vlk12 bootloader

2,290 Views
daafies
Contributor II


does anyone have an example/demo for a bootloader on the mk22fn1m0vlk12 platform?

thanks very much

Labels (2)
0 Kudos
Reply
4 Replies

2,099 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello david,

Does this can help you ? Kinetis Bootloader to Update Multiple Devices in a Network for Cortex-M4


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,099 Views
daafies
Contributor II

hi Alice,

thanks. you dont happen to have this ported to mk22fn1m0vlk12 already do you?

david

0 Kudos
Reply

2,099 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

Sorry i have not port it to this chip , i think it is easy , you can try it , if there is

something question , you can tell me without any hesitate.

BR

Alice

0 Kudos
Reply

2,099 Views
mjbcswitzerland
Specialist V

Hi

The uTasker project includes boot loaders for the K22FN1Mx12:

- UART iHex/SREC/KBOOT/AN2295

- USB-MSD/KBOOT/CDC/HIDloader.exe (device)
- USB memory stick (Host)

- SD card

Each can be selected by a define and mixed as desired to have mutiple loaders operating in parallel (including USB host or device modes automatically detected).

Builds with GCC, IAR, Keil, Green Hills, Rowley Crossworks, KDS, CW 10.x, Atollic or VisualStudio for simulation.

Regards

Mark

0 Kudos
Reply