mingw32-make: *** [HORNO2.elf] Error1 help me!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mingw32-make: *** [HORNO2.elf] Error1 help me!

3,248件の閲覧回数
alejandro_df
Contributor I

I have an application where I am using kl25. with usb stack with  processor expert does not send a single error in the code but when copilar just sends me the following error:
Description Resource Path Location Type
mingw32-make: *** [HORNO2.elf] Error 1 HORNO2 C / C + + Problem



Message was edited by: Monica Arvizu

0 件の賞賛
返信
3 返答(返信)

2,064件の閲覧回数
apanecatl
Senior Contributor II

I suggest you include your project code to review it, the mingw32-make error is quite common and not very specific, also include the part you are using, i.e.: MK60DN512

0 件の賞賛
返信

2,064件の閲覧回数
alejandro_df
Contributor I

Sorry. the warnings are from another project. my project does not send a single warning

0 件の賞賛
返信

2,064件の閲覧回数
Monica
Senior Contributor III

Hola Alejandro!

I removed the warning section from your post to avoid confusion...let me know if any concern.

Best regards,

Monica.

0 件の賞賛
返信