meterlib1ph_cfg I_MAX, U_MAX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

meterlib1ph_cfg I_MAX, U_MAX?

1,401 Views
hyunwoochoi
Contributor I

Hello,

My project is based on _twr_emeter_demo(old one with KM34 128 series).

I can see a document: DRM143 Kinetis-M One-Phase Power Meter Reference Design.

Here is the question details.

Does U_MAX and I_MAX come from this schematic?

Then U_MAX should be 325.26V as it mentioned?

However, on page 25, it mentioned:286V not 325.26V.

I am not sure which value is correct one.

If my circuit use smaller register values such as two 150 Kohm instead of four 150 Kohm, then U_MAX value should be changed? then how?

There is no note about I_MAX though. Anyone know how to pick the value?

Thanks,

Hyunwoo

- page 25,

pastedImage_3.png

- page 13,

pastedImage_0.png

Labels (1)
0 Kudos
Reply
1 Reply

1,297 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

The U_MAX has two factors could affect that value, one is the meter AC_DC SMPS related circuit design, which should match with the meter spec design requirement, the other one to meet the current measurement requirement.

The I_MAX value is based on hardware design and the ADC measure range (VREFH voltage), the ADC measurement value should not exceed the measure range to make current value in a range. The hardware schematics (shunt resistor value) also affect the I_MAX value, which also affect the U_MAX value.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply