memory question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

memory question

2,169件の閲覧回数
todtodf
Contributor I

Dear  Expert:

is there a bit-band region of SRAM in KE02(not AIPS)? below is from the KE02 reference manual:

pastedImage_1.png

in ke06 refence manual,it is clear description about the SRAM bit_band:

pastedImage_2.png

thanks for your great support.

0 件の賞賛
返信
4 返答(返信)

2,073件の閲覧回数
todtodf
Contributor I

Dear  Expert:

thanks for your support.

But you can download the AN4838.pdf from www.nxp.com

The is a description below:

pastedImage_2.png

0 件の賞賛
返信

2,073件の閲覧回数
mjbcswitzerland
Specialist V

Hi

KE04 and KE06 are indeed exceptions in that there is really a bit-banding capability in the upper SRAM (I didn't think that any Kinetis Cortex-m0+ parts had it), however it is IS NOT implemented in the KE02.

Regards

Mark

0 件の賞賛
返信

2,073件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Actually all KE families employ Bit Manipulation Engine (BME) techniques to support bit banding.

0 件の賞賛
返信

2,073件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The KE series does not implement bit-banding (the description is probably a generic one that is used in all documents).

However it does include a bit-manipulation engine which does more or less the same thing as bit-banding (even with more flexibility, although using different address calculations). Unfortunately it can only access peripherals on the KE parts and not SRAM....

Regards

Mark

0 件の賞賛
返信