max external SDRAM size on K66F ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

max external SDRAM size on K66F ?

1,179件の閲覧回数
pwalh
Contributor I

Hi,

my company developed a device based on LPC1788. It features a two-chips 128MB SDRAM. The device is already in production.

We are starting a new project in which we want to develop a new device with cloud connectivity. In this project, security is critical. Thus we are planning to use a Kinetis K66F which supports hardware encryption.

We also need at least 256MB SDRAM. 512MB would be best. 

In the K66 Ref Manual, section 35.5.1, it is said that "The maximum SDRAM address size is 128 Mbits". Does it mean that the maximum memory size is 16MB ? Or perhaps is it 16MB per chip select ? Is it at all possible to interface high capacity (512MB) SDRAM with a K66F ? 

Thank you in advance for your help

0 件の賞賛
返信
1 返信

1,078件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Pierre Walhin,

The K66 can't support the SDRAM whose size beyond the 16 Mb.

Hope this is clear.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信