lwIP & PE & K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lwIP & PE & K60

2,312 Views
kizo
Contributor I

Hello,

I’ve found KSDK on your website in which are examples using lwIP stack, but neither of these examples use processor expert nor K60 MCU. Is there any examples with lwIP with PE on KDS or CW using MK60DN512Z?

Thanks,

Zoran

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,744 Views
antonioconcio
NXP Employee
NXP Employee

Hi Zoran,

In the next KSDK release 1.1, scheduled on December 16th, there will be support for MK60DN512.

Kinetis SDK supports the following IDEs:

For more info on KSDK please refer HERE.

Hope that helps,

Antonio

1,744 Views
dave408
Senior Contributor II

As far as I can tell, KSDK 1.1 did not include anything with PEx and lwIP.  There's the lwIP example, but I looked over the documentation included with the KSDK and the example only shows how to compile and run it.

That said, Antonio, I am in the process of figuring out how to get a project together that gives me simple TCP/IP communication and leverages PEx for all of the other peripherals on the chip.  I'll try to remember to post my findings here, should I complete that task.

0 Kudos
Reply