ls1021a/ls1028a device tree (tsn)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1021a/ls1028a device tree (tsn)

1,597 Views
trp
Contributor I

Hi!

I am working on the device tree for the ls1028a where we are using SPI3 with an attacted KSZ8567 ethernet switch.

As I understand it, the ls1021a (tsn) variant is pretty similar to our custom-board in the sense that it also has an external ethernet switch. There, I downloaded the software for the ls1021a to lookat the device tree to get some ideas.. However, the package I downloaded did not contain any DTS-files. I cannot find it in the LSDK19.09 either.

It is possible to share the device tree of ls1021a here, or point me in the right direction where I can find it? Hopefully, I can also understand which driver(s) to include in the kernel config..

Help is appreciated!

Best rgds,

Tom Roar Pedersen

0 Kudos
Reply
1 Reply

1,507 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could refer to ls1021atsn dts file provided in OpenIL, please refer to the attached dts file.

You could refer to "Chapter 2 Getting started" in https://www.nxp.com/docs/en/user-guide/OPEN-LINUX-IND-UM-1-7-1.pdf to download OpenIL and run the following command to get Linux Kernel source code in output/build/linux-OpenIL-v1.7-linux-202001.

$ make nxp_ls1021atsn_defconfig

$ make linux

Then refer to arch/arm/boot/dts/ls1021a-tsn.dts in Linux Kernel source code.

0 Kudos
Reply