kw40z pin define question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kw40z pin define question

1,529件の閲覧回数
shinezen
Contributor III

In this datasheet (MKW40Z Reference Manual)   have ADC0_Dm0 pin define is ADC Channel 0 Differential Input negitive.  but FRDM-KW40Z Schematics this pin ADC0_DP0 was used by ADC0_SE1/POT.

so this datasheet (MKW40Z Reference Manual) is old version??

1 返信

1,222件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Actually both the datasheet & user maunal and schematic are correct. Please make reference from the table of below:

pastedImage_0.png

Per the setting of "SCxn[DIFF]= 0", this means that the input will be single ended and there you'll find the DM channels used as single eneded.

0 件の賞賛
返信