kinetis process expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetis process expert

2,497 Views
diego_ambroggi
Contributor I

Hello everybody

It's my first experience with NXP microcontrollers.

I chose Kinetis EA for my embedded application.

So I installed S32DS tool for a FRDM-KEAZ64Q64  evaluation KIT.

I tried some example projects and now I need to start my own application.

I want to use Processor expert to simply configure pinout, drivers ecc., but no one "*.pe" file are present in examples.

Have some tips for me? :smileysad:

Thanks

Diego

Labels (1)
2 Replies

2,264 Views
mjbcswitzerland
Specialist V

Hi Diego

See links below for KEA8 and KEA64 support in the uTasker project (as open source or professional versions).
It has chip simulation and doesn't need configuration tools to set up immediately working projects, which can be used with S32, KDS or MCUXpressor (or various others).

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
Kinetis KEA64:
- http://www.utasker.com/kinetis/FRDM-KEAZ64Q64.html
- http://www.utasker.com/kinetis/TRK-KEA64.html
- http://www.utasker.com/kinetis/TRK-KEA8.html

S32 Design Studio: http://www.utasker.com/kinetis/compilers.html#S32

Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html

2,264 Views
miduo
NXP Employee
NXP Employee
Hello,

We recommend S32 Design Studio to work with the KEA family, because this devices are oriented to automitive applications.  
However unfortunately, KEAZ64 and KEAZ8 are old MCUs and at the moment there is no plan to add SDK package in S32DS
 for this devices.  
In this case KDS is the IDE that support those MCUs with Processor Expert, but this IDE was replaced by MCUXpresso IDE. 
And the support for KEA devices got limited to KDS (or S32DS).  So if you really to use the PE, the KDS is the only choise.