kinetis library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetis library

Jump to solution
4,017 Views
josemartinez
Contributor III

Hello,

does anybody know if there is an eagle library for Kinetis K40 and K20 microcontroller??

Thanks,

Jose

Labels (1)
1 Solution
2,915 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I am not sure what are you looking for. but we have the Capture Symbol (orcad) and the Footprint (land pattern) Cadence Allegro(dra) for some of our MCU, you can find this information under the   icon that is show when you search a part number. For instance, if you search the part number MK40DN512VMD10 on the ordenable part  you will get the following result

http://www.freescale.com/webapp/search/MainSERP.jsp?SelectedAsset=Orderable%20Parts#breadcrumb_ancho...

and on this page just make click on the   icon to get  MK40DN512VMD10 Information

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MK40DN512VMD10&buyNow=t...

Where you can get information about the package, Environmental and Compliance etc

For different part number you just need to put the correct part number and follow the same process

I hope this will help you.

Regards

Vicente

View solution in original post

0 Kudos
Reply
4 Replies
2,915 Views
Monica
Senior Contributor III

Hello Jose,

did that answered your question? Please don't forget to keep us posted :smileywink:

Best regards,

Monica

0 Kudos
Reply
2,915 Views
josemartinez
Contributor III

Yes I solved the problem with this answer

Thanks

Jose

2,915 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I am not sure what are you looking for. but we have the Capture Symbol (orcad) and the Footprint (land pattern) Cadence Allegro(dra) for some of our MCU, you can find this information under the   icon that is show when you search a part number. For instance, if you search the part number MK40DN512VMD10 on the ordenable part  you will get the following result

http://www.freescale.com/webapp/search/MainSERP.jsp?SelectedAsset=Orderable%20Parts#breadcrumb_ancho...

and on this page just make click on the   icon to get  MK40DN512VMD10 Information

http://www.freescale.com/webapp/search.partparamdetail.framework?PART_NUMBER=MK40DN512VMD10&buyNow=t...

Where you can get information about the package, Environmental and Compliance etc

For different part number you just need to put the correct part number and follow the same process

I hope this will help you.

Regards

Vicente

0 Kudos
Reply
2,915 Views
davidsun
Contributor II

I followed your instruction and I found

MKL04Z8VFK4 Information
Product Summary Page

   General Information
Package Information
Environmental and Compliance Information
  Manufacturing Information
  Ordering Information
Product/Process Change Notice (PCN)
Operating Characteristics
   Reliability Data Lookup

continue Package information

I got 98ASA00474D.pdf from the following link. may be I have been using TI's chip for a long time. I feel it is hard to find useful information for this chip, I couldn't even find a land pattern in PDF format, in user manual, or data sheet. if not for the cost issue, I would keep using TI MSP chip. I guess I have to create the layout symbol from the chip package. it is a pain in the neck.

thanks,

David

Package Information

ParameterValue
Package Type and Termination CountQFN 24
Package Description and Mechanical DrawingQFN MAP 24 4*4*1 P0.5
Device Weight(g).01580
Package Length (nominal)(mm)4.000
Package Width (nominal)(mm)4.000
Package Thickness (nominal)(mm)1.000
Tape & ReelNo
0 Kudos
Reply