kinetis bootloader for k61

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kinetis bootloader for k61

2,148件の閲覧回数
antonioserrano
Contributor I

Hello,

I'm very new to Kinetis microcontrollers and NXP Solutions in general and I'm trying to develop a custom bootloader application for the MK61FN1M0xxx15. I've been browsing through the offered tools and saw that NXP provides a Kinetis Bootloader for Kinetis devices. As part of the solution there are CMSIS based target definitions, but not all processors are supported. Reading the documentation it says that porting the Kinetis Bootloader to processors not listed in the sample targets requires having system_<platform>.c/h definitions along with other files which are supposed to be obtainable from the device page. I have failed in getting those files.

Basically I would like guidance on how to start migrating the kinetis bootloader for that specific processor so then I can modify it to my needs. Any help or ideas are welcomed! I'm very lost with this platform...

Thanks in advanced.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,980件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Take a look at http://www.utasker.com/kinetis/EMCRAFT_K61F150M.html
and
http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

There are various boot loaders for the K61 (SD card, Kboot, UART, USB, memory stick, Ethernet) available that need no porting. You can simulate them in (approx.) real-time in the K61 simulator for adapting, testing and debugging to simplify any customisation if needed.

Regards

Mark
 

0 件の賞賛
返信

1,980件の閲覧回数
antonioserrano
Contributor I

Hi Mark,

Thank you very much for your kind reply. Is there a possibility of using the Kinetis Booloader Project?

What seems to be missing is the CMSIS files for the processor. Do you know where can I get that?

0 件の賞賛
返信

1,980件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Antonio Serrano,

Please check the attachment.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,980件の閲覧回数
mjbcswitzerland
Specialist V

Hi Antonio

Sorry, I have no idea where such a file can be located. You may need to write one by copying a close one and making any necessary adjustments.

Regards

Mark

0 件の賞賛
返信