kinetic design studio debugging issue with MKE04Z64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetic design studio debugging issue with MKE04Z64

1,233 Views
ravindra
Contributor I

Hi,

i am facing issue while software debugging by using kinetis design studio IDE with J link segger programmer and MKE04Z64 MCU

i am able to burn programme into mcu but problem comes only for debugging the code.

kindly help us to sort out the issue

0 Kudos
Reply
1 Reply

1,215 Views
nxf58904
NXP Employee
NXP Employee

Hi,

First,we use a blinking example to make sure that your chip can work well.

Then,check the initialization of the chip . For example, if you use systick ,but you didn't init it ,the issue will happen.

 

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply