k65 HSRUN to RUN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

k65 HSRUN to RUN

1,600 Views
steverobalino
Contributor I

Im using the K65 in HSRUN mode (180mhz)

I need to write configuration data to a sector of flash

so for a short time I need to switch out of HSRUN to slower clock speed in order to erase /program the flash

where do I find description and examples?

0 Kudos
Reply
1 Reply

1,282 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please refer KSDK V1.3 [power_manager_hal_demo] demo, which shows how to change working mode from HSRUN to RUN mode. The default demo path is :

C:\Freescale\KSDK_1.3.0\examples\twrk65f180m\demo_apps\power_manager_hal_demo


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply