k64 usb err

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k64 usb err

1,516件の閲覧回数
dugg
Contributor II

hello everyone

      during the communication of the USB,i pull up the USB line, the routine enter into the interrupt of usb err.

      but,i read the register of USB0_ERRSTAT,it's value is 0x00,

      how can i know  the reason of the err?

ラベル(1)
0 件の賞賛
返信
1 返信

1,354件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

In order to understand the results from the those registers I recommend that you take a look at the Reference Manual and sections 46.4.9, 46.4.10 and 46.4.11. These sections explain the bits in those registers, normally a 0x00 is read after a reset.

In addition, if you are working with USB I would also recommend that you take a look at SDK examples that focus on USB for the K64, as a reference.

Let me know if you have questions with the above mentioned,

Thank you,

Sabina