k64 sram User use area?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k64 sram User use area?

1,987件の閲覧回数
johnbaker
Contributor IV

Soooooooooooo,

What address space can I use on my MK64FN1M0VDC12 can use without bricking my board??  (Apparently I should not have started writing stuff at 0x1FFF0000)   :-(

John Baker

0 件の賞賛
返信
2 返答(返信)

1,861件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello John:

The available RAM space is mentioned in the Reference Manual:

K64_mem.png

However, disregarding of memory range, there is no way you can brick your device by writing to any address. Why do you think it is bricked?


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,861件の閲覧回数
johnbaker
Contributor IV

Hmmmmm,

That is the address we came up with and are using. There must be something else going on then.

Again, thanks for the quick response!

John

0 件の賞賛
返信