k64 sram User use area?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

k64 sram User use area?

2,113 Views
johnbaker
Contributor IV

Soooooooooooo,

What address space can I use on my MK64FN1M0VDC12 can use without bricking my board??  (Apparently I should not have started writing stuff at 0x1FFF0000)   :-(

John Baker

0 Kudos
Reply
2 Replies

1,987 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello John:

The available RAM space is mentioned in the Reference Manual:

K64_mem.png

However, disregarding of memory range, there is no way you can brick your device by writing to any address. Why do you think it is bricked?


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,987 Views
johnbaker
Contributor IV

Hmmmmm,

That is the address we came up with and are using. There must be something else going on then.

Again, thanks for the quick response!

John

0 Kudos
Reply