k64 serial com munication stopped working after exiting vlps mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k64 serial com munication stopped working after exiting vlps mode.

1,584件の閲覧回数
hunglam
Contributor II

HI,

In my application I need to switch periodically between run mode and very low power stop mode. I use the RTC alarm interrupt to exit the stop mode  which works just fine. However, after exiting the stop mode the serial communication stops working. Do I need to deinit the uart before entering the stop mode and initializes it again after exiting? hope someone can help me? thanks

0 件の賞賛
返信
2 返答(返信)

1,475件の閲覧回数
mjbcswitzerland
Specialist V

Hi

It is not necessary to re-initialie anything at the UART after exiting VLPS.

See the following https://community.freescale.com/message/421247#421247 

Regards

Mark

0 件の賞賛
返信

1,475件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mark,

   Thank you for your reply, linker should be:

https://community.nxp.com/message/421247#421247

  Otherwise, it will be the wrong link.

Best Regards,

Kerry

0 件の賞賛
返信