k22 usb device descriptors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k22 usb device descriptors

2,056件の閲覧回数
584069980
Contributor I

I am using the MCU MK22FN512VLL12.My problem is that I can receive 8-byte device requests,
but the device descriptors can't be sent out. And Cause some Error flags, PIDERR BTOERR BTSERR

so what is the possible reason and how to solve this problem ?

0 件の賞賛
返信
3 返答(返信)

1,928件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Cai,

 

Could you please provide more details of your application? I recommend you to check the reference manual in chapter 43.4.11 Error Interrupt Status register (USBx_ERRSTAT). There you will find description about each error source that you might be falling into.

 

Best regards,

Felipe

0 件の賞賛
返信

1,928件の閲覧回数
584069980
Contributor I

   Thanks !

   

   When the PC recognizes that there is a USB device inserted, it will send a device request. K22    will send  device descriptors to the PC after receiving an 8-byte device request. That's the    problem. K22 can't send device descriptors.The PC will not be able to enter the next    configuration.

   

   I know the reason of these errors, but I don't know how to deal with  them。Which registers need    to be modified

   

   Best regards,

   Cai

0 件の賞賛
返信

1,928件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Cai,

 

If you have incorrect data being sent or expected the transfers will fail, which is presumably what is happening. Please check the below thread from a customer that was experiencing Turnaround Timeout error as well.

https://community.nxp.com/thread/308999 

 

In addition, I recommend you to monitor USB traffic with a USB analyzer.

 

Best regards,

Felipe

0 件の賞賛
返信