k20 not enabling interrupts after transfer from bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

k20 not enabling interrupts after transfer from bootloader

2,592件の閲覧回数
waynewilburn
Contributor II

I have a custom bootloader that was designed for the KL16 and I have ported it to the K20.  I used Processor Expert (KDS) to design both versions of the code.  My bootloader is at address 0x0000 and the application is at 0x3000.

The code in the bootloader that actually does the jump is:

void Execute_JumpToApplication( void )
{
__DI();
SCB_VTOR = (uint32_t)APPLIC_BASE_ADDR;
uint32_t startup;
startup = ((uint32_t*)APPLIC_BASE_ADDR)[0];
__set_SP(startup);
startup = ((uint32_t*)APPLIC_BASE_ADDR)[1];
((void(*)(void))startup)();
}

When I load my application with a debugger, interrupts are enabled correctly.  When I transfer control from my bootloader, interrupts do not appear to be enabled.  Even my timer interrupt does not work.  Here is the initialization code from Cpu.c.  I have commented most of the initialization functions.  Only TI1_Init() and BitsIOLdd1_Init() remain.  All of my interrupt code was set to priority 8.  Any suggestions with how to proceed?

void PE_low_level_init(void)
{
#ifdef PEX_RTOS_INIT
PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/* Initialization of the SIM module */
/* Initialization of the RCM module */
/* RCM_RPFW: RSTFLTSEL=0 */
RCM_RPFW &= (uint8_t)~(uint8_t)(RCM_RPFW_RSTFLTSEL(0x1F));
/* RCM_RPFC: RSTFLTSS=0,RSTFLTSRW=0 */
RCM_RPFC &= (uint8_t)~(uint8_t)(
RCM_RPFC_RSTFLTSS_MASK |
RCM_RPFC_RSTFLTSRW(0x03)
);
/* Initialization of the FTFL_FlashConfig module */
/* Initialization of the PMC module */
/* PMC_REGSC: ACKISO=0,BGBE=0 */
PMC_REGSC &= (uint8_t)~(uint8_t)(
PMC_REGSC_ACKISO_MASK |
PMC_REGSC_BGBE_MASK
);
/* PMC_LVDSC1: LVDACK=1,LVDIE=0,LVDRE=1,LVDV=0 */
PMC_LVDSC1 = (uint8_t)((PMC_LVDSC1 & (uint8_t)~(uint8_t)(
PMC_LVDSC1_LVDIE_MASK |
PMC_LVDSC1_LVDV(0x03)
)) | (uint8_t)(
PMC_LVDSC1_LVDACK_MASK |
PMC_LVDSC1_LVDRE_MASK
));
/* PMC_LVDSC2: LVWACK=1,LVWIE=0,LVWV=0 */
PMC_LVDSC2 = (uint8_t)((PMC_LVDSC2 & (uint8_t)~(uint8_t)(
PMC_LVDSC2_LVWIE_MASK |
PMC_LVDSC2_LVWV(0x03)
)) | (uint8_t)(
PMC_LVDSC2_LVWACK_MASK
));
/* SMC_PMPROT: ??=0,??=0,AVLP=0,??=0,ALLS=0,??=0,AVLLS=0,??=0 */
SMC_PMPROT = 0x00U; /* Setup Power mode protection register */
/* Common initialization of the CPU registers */
/* NVICIP8: PRI8=0 */
NVICIP8 = NVIC_IP_PRI8(0x00);
/* GPIOD_PDDR: PDD&=~0x40 */
GPIOD_PDDR &= (uint32_t)~(uint32_t)(GPIO_PDDR_PDD(0x40));
/* ### Asynchro serial "DebugUART" init code ... */
//DebugUART_Init();
/* ### InternalI2C "Vpi" init code ... */
//Vpi_Init();
/* ### BitIO_LDD "BitIoLdd1" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
//(void)BitIoLdd1_Init(NULL);
/* ### IntFLASH "FLASH" init code ... */
//FLASH_Init();
/* ### GPIO_LDD "BitsIoLdd1" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
(void)BitsIoLdd1_Init(NULL);
/* ### BitIO_LDD "BitIoLdd2" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
//(void)BitIoLdd2_Init(NULL);
/* ### BitIO_LDD "BitIoLdd3" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
//(void)BitIoLdd3_Init(NULL);
/* ### BitIO_LDD "BitIoLdd4" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
//(void)BitIoLdd4_Init(NULL);
/* ### ExtInt_LDD "ExtIntLdd1" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
//(void)ExtIntLdd1_Init(NULL);
/* ### ADC "TempADC" init code ... */
//TempADC_Init();
/* ### SPIMaster_LDD "SPI_LDD" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
//(void)SPI_LDD_Init(NULL);
/* ### TimerInt_LDD "TI1" component auto initialization. Auto initialization feature can be disabled by component property "Auto initialization". */
(void)TI1_Init(NULL);
/* Enable interrupts of the given priority level */
__set_BASEPRI(0U);
}

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,567件の閲覧回数
waynewilburn
Contributor II

So I’ve tried both __EI() and __enable_interrupt() at the end of low_level_init and neither work

0 件の賞賛
返信

2,587件の閲覧回数
jay_heng
NXP Employee
NXP Employee

It seems that global IRQ is disabled in bootloader and it is not enabled again in application.

Global IRQ is enabled by default, that's why you can debug application only properly

0 件の賞賛
返信

2,583件の閲覧回数
waynewilburn
Contributor II

So I added an __EI() statement at the end of Cpu.c but that did not fix the problem.  I thought that the __set_BASEPRI statement enabled the interrupts??

0 件の賞賛
返信

2,571件の閲覧回数
ErichStyger
Specialist I

No, BASEPRI only sets the base priority of interrupts to be masked, see https://mcuoneclipse.com/2016/08/14/arm-cortex-m-interrupts-and-freertos-part-1/

Erich

0 件の賞賛
返信