input frequency capture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

input frequency capture

1,058 Views
pandi
Contributor III

Hi everyone

how to configure input capture mode KV31F512VLL12 guide me and if  you have sample program give to me  help for us.

I `m trying this code correct or not if not means any changes  guide me 

void TIM1_init(void) {

 

SIM->SCGC5 |= SIM_SCGC5_PORTB(1);

PORTB->PCR[0] = PORT_PCR_MUX(0x3); // Set pin as ALT3 (TIM1_CH1)

SIM->SCGC6 |= SIM_SCGC6_FTM1(1);

FTM1->SC = 0;

FTM1->MOD = 1999;

FTM1->CONTROLS[1].CnSC = FTM_CnSC_MSB_MASK | FTM_CnSC_ELSB_MASK;

FTM1->CONTROLS[1].CnV = 1000;

FTM1->SC = FTM_SC_PS(7) | FTM_SC_TOF(1);

}

 

void TIM2_init(void) {

// Enable clock for PORTA

SIM->SCGC5 |= SIM_SCGC5_PORTA_MASK;

PORTA->PCR[1] = PORT_PCR_MUX(0x3); // Set pin as ALT3 (TIM2_CH1)

SIM->SCGC6 |= SIM_SCGC6_FTM2(1);

FTM2->SC = 0;

FTM2->CONTROLS[1].CnSC = FTM_CnSC_ELSA_MASK | FTM_CnSC_ELSB_MASK |FTM_CnSC_CHIE_MASK;

FTM2->SC = FTM_SC_PS(7) | FTM_SC_TOF(1);

NVIC_EnableIRQ(FTM2_IRQn);

}

void FTM2_IRQHandler() {

// Clear channel flag

FTM2->CONTROLS[1].CnSC &= ~FTM_CnSC_CHF_MASK;

 

if (gap == 0) {

counter0 = FTM2->CONTROLS[1].CnV;

gap = 1;

else {

counter1 = FTM2->CONTROLS[1].CnV;

if (counter1 > counter0) {

Counter = counter1 - counter0;

Frequency = 10000 / Counter;

else {

Counter = counter1 + 0xFFFF - counter0 + 1;

Frequency = 10000 / Counter;

}

counter0 = counter1;

}

}

                                            Thank you

BR

PANDI

0 Kudos
Reply
1 Reply

1,018 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Pandi,

When you input a tested signal to FTM2_CH1 pin, can you enter the FTM2_IRQHandler()?

If you can, it is okay, in the FTM2_IRQHandler(), you can check the overflow flag, if it is set, just clear the flag, and add 0xFFFF. While, you can assign the FTM2_MOD register to 0xFFFF in the FTM2 init code.

Void FTM2_ISR(void)
{

if(FTM2_STATUS&0x02)
{

FTM2_STATUS&=0xFD;
tempPrev=temp;
temp=FTM0_C0V; //read FTM0 counter register
diff=temp-tempPrev;

if(FTM2_SC&0x80)

{
diff=0xFFFF+diff;

FTM2_SC&=~(0x80); //clear overflow flag
GPIOC_PTOR=0x80;
asm("nop"); //set a break point here
}
}

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply