in the "fsl_flash.h" file:

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

in the "fsl_flash.h" file:

485 次查看
nguyenhuytung
Contributor I

In the "fsl_flash.h" file:

enum _flash_execute_in_ram_function_constants

{

    kFLASH_ExecuteInRamFunctionMaxSizeInWords = 16U, /*!< Max size of execute-in-ram function.*/

    kFLASH_ExecuteInRamFunctionTotalNum = 2U         /*!< Total number of execute-in-ram functions.*/

};

Anyone know why the max size of execute-in-ram function is 16?

I'm using FRDM-KV31F board.

0 项奖励
回复
0 回复数