in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

723件の閲覧回数
kalpananachneka
Contributor I

in MKM33Z128XXX microcontroller, can we use multiple Uarts simultaniously? If yes , may I get the sample code for the same .

ラベル(1)
0 件の賞賛
返信
1 返信

602件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kalpana,

Definitely, they are independent.

And I'd highly recommend you to refer to the KSDK development kit which provides the several kinds of the demo applications and the demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution and the capabilities of the peripheral drivers.

KSDK:

Software Development Kit for Kinetis MCUs|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信