i2s initialization issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i2s initialization issue

ソリューションへジャンプ
4,029件の閲覧回数
deepakbhagat
Contributor II

I am working on k70 tower kit interface with TWR-AUDIO-SGTL. I am working on i2s protocol for the first time. so can you guide me what initalization i need to do for i2s in k70 if i have to playback wave file with following header that is displayed. It would be gr8 help if you can help me with i2s initialization. We are going to supply Mclk, Bit CLk and FS from K70 to SGTL5000. The on board oscilator is removed for our application.

I am not using MQX for our application we are working on standalone driver. Actually i am new to i2s i haven't configured i2s earlier. i am facing problem in configuring the FS to 44.1khz. We are using Keil for development.

ラベル(1)
1 解決策
3,728件の閲覧回数
JerryFan
NXP Employee
NXP Employee

Please refer mqx\examples\i2s_demo\iar\i2s_demo_twrk70f120m. This demo set K70 SAI as master, while it is easily to configure it as slave using ioctl(fd, IO_IOCTL_I2S_SET_MODE_SLAVE).

Even you are not use MQX, this can be a reference.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,728件の閲覧回数
Monica
Senior Contributor III

Hello Deepakbhagat,

was that suggestion helpful? Please let us know.

Regards,

Monica

0 件の賞賛
返信
3,728件の閲覧回数
deepakbhagat
Contributor II

Yes my I2S is working fine and running with the help of Adam Pitak.

3,729件の閲覧回数
JerryFan
NXP Employee
NXP Employee

Please refer mqx\examples\i2s_demo\iar\i2s_demo_twrk70f120m. This demo set K70 SAI as master, while it is easily to configure it as slave using ioctl(fd, IO_IOCTL_I2S_SET_MODE_SLAVE).

Even you are not use MQX, this can be a reference.

0 件の賞賛
返信