i2c bus reads 2 bytes instead of one?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2c bus reads 2 bytes instead of one?

969 Views
alexandradickie
Contributor I

I'm using the KEAZ128 and I just downloaded the quick start package which has a bunch of test drivers in it. I started using the polling i2c driver and noticed that its reading two bytes out of the i2c register called instead of one? Has anyone else encountered this problem with this code?  Here is the read function from the file: 

uint8_t I2C_MasterReadWait(I2C_Type *pI2Cx,uint16_t u16SlaveAddress,uint8_t *pRdBuff,uint32_t u32Length)
{
uint32_t i;
uint8_t u8ErrorStatus;

/* send start signals to bus */
u8ErrorStatus = I2C_Start(pI2Cx);

/* send device address to slave */
u8ErrorStatus = I2C_WriteOneByte(pI2Cx,u16SlaveAddress | I2C_READ);

/* if no error occur, received the correct ack from slave
continue to send data to slave
*/
/* dummy read one byte to switch to Rx mode */
I2C_ReadOneByte(pI2Cx,&pRdBuff[0],I2C_SEND_ACK);

if( u8ErrorStatus == I2C_ERROR_NULL )
{
for(i=0;i<u32Length-1;i++)
{
u8ErrorStatus = I2C_ReadOneByte(pI2Cx,&pRdBuff[i],I2C_SEND_ACK);
if( u8ErrorStatus != I2C_ERROR_NULL )
{
return u8ErrorStatus;
}
}
u8ErrorStatus = I2C_ReadOneByte(pI2Cx,&pRdBuff[i],I2C_SEND_NACK);
}
/* send stop signals to bus */
u8ErrorStatus = I2C_Stop(pI2Cx);
return u8ErrorStatus;
}

0 Kudos
Reply
1 Reply

808 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi
Please refer the "Figure 31-42. Typical I2C interrupt routine" in KEA128RM.

Dummy read.png

u8ErrorStatus = I2C_ReadOneByte(pI2Cx,&pRdBuff[i],I2C_SEND_NACK);  is used to read one byte out of the i2c register.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply