i can not debbug in the KL25Z FRDM...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i can not debbug in the KL25Z FRDM...

ソリューションへジャンプ
3,700件の閲覧回数
josealonsovalle
Contributor III

Hi, I am new in this of the kinetis microcontroller, and i have the FRDM KL25Z but when i wanna debbug, codewarrior shows  a error alert....Can somebody help me please??...

ddd.PNG.png

ラベル(2)
1 解決策
3,311件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jose,

have you switched to the SDA debug application? It looks like you are running the wrong firmware for debugging.

See

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

元の投稿で解決策を見る

5 返答(返信)
3,311件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

By default the firmware running in the OpenSDA device is the MSD, you have to program the debug application into OpenSDA.

Follow the OpenSDA User Guide.

http://cache.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf?fpsp=1&WT_TYPE=Users Guides&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

  1. Getting into Bootloader Mode
  2. Program the P&E Debug Application

Then CW will detect your debugger device.

Best Regards,

Luis

3,312件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jose,

have you switched to the SDA debug application? It looks like you are running the wrong firmware for debugging.

See

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

3,311件の閲覧回数
josealonsovalle
Contributor III

Thanks bro, already i can debbug my board....

0 件の賞賛
返信
3,311件の閲覧回数
nasreenshaikh
Contributor III

HI Jose,

     Which device are you using for debugging? Multilink, Cyclone pro, Jtag, or OSBDM? you will need the drivers for whichever debugging tool you are using.

0 件の賞賛
返信
3,311件の閲覧回数
josealonsovalle
Contributor III

Hi, i believe that is the OPEN SDA, and i did install the drivers of the FRDM. The KL25 FRDM don't need a BDM..

0 件の賞賛
返信