how many ADC sample can use in the MKE06Z128VLK4? I cannot read 9th(SampleGroup[8])ADC data (already used 8 ADC). Plaese help!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how many ADC sample can use in the MKE06Z128VLK4? I cannot read 9th(SampleGroup[8])ADC data (already used 8 ADC). Plaese help!

870件の閲覧回数
aaron0312
Contributor I

void Adc_init(void)
{
/* ADC initialization */
MyADCPtr = ADC_Init((LDD_TUserData *)NULL); /* Initialize the device */
Vr_temp_PutVal(1);
/* Create 8-sample group */
SampleGroup[0].ChannelIdx = 0U; /* ADC of Vref */
SampleGroup[1].ChannelIdx = 1U; /* ADC of T1 */
SampleGroup[2].ChannelIdx = 2U; /* ADC of T2 */
SampleGroup[3].ChannelIdx = 3U; /* ADC of T3 */
SampleGroup[4].ChannelIdx = 4U; /* ADC of T4 */
SampleGroup[5].ChannelIdx = 5U; /* ADC of T5 */
SampleGroup[6].ChannelIdx = 6U; /* ADC of T6 */
SampleGroup[7].ChannelIdx = 7U; /* ADC of VCP */
SampleGroup[8].ChannelIdx = 8U; /* ADC of current shunt */

PE_Error = ADC_CreateSampleGroup(MyADCPtr, (LDD_ADC_TSample *)SampleGroup, 8U); /* Set created sample group */
if(PE_Error != 0)
{
SS_ERROR=0x71;
}

}

void Adc_Pro(void)
{

static uint8_t ADCAverge;
uint8_t ADC_Cunter;
PE_Error = ADC_StartSingleMeasurement(MyADCPtr); /* Start continuous measurement */
if ( PE_Error )
{
SS_ERROR=0x71;
}
while (!ADC_GetMeasurementCompleteStatus(MyADCPtr)) {}; /* Wait for conversion completeness */
PE_Error = ADC_GetMeasuredValues(MyADCPtr, (LDD_TData *)MeasuredValues); /* Read measured values */
if ( PE_Error )
{
SS_ERROR=0x71;
}

0 件の賞賛
返信
1 返信

783件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 育鈞,

Sorry for the late reply!

Number of items in the sample definition array. Must be less than or equal to ComponentName_MAX_HW_SAMPLE_COUNT.

SampleCount.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信