hi everybody ,im working with te kl25z microcontroller i need to do 4 differential adc ,i menaged to find 2 pair the PTE20,PTE21 and the PTE22,PTE23 but where are two more pairs i dosent find them help ???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hi everybody ,im working with te kl25z microcontroller i need to do 4 differential adc ,i menaged to find 2 pair the PTE20,PTE21 and the PTE22,PTE23 but where are two more pairs i dosent find them help ???

1,091 Views
ilancohen
Contributor II

hi everybody ,im working with te kl25z microcontroller i need to do 4 differential adc ,i menaged to find 2 pair the PTE20,PTE21 and the PTE22,PTE23 but where are two more pairs i dosent find them help ???

Labels (1)
2 Replies

951 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello,

On the KL25 there are only two pairs of differential analog inputs available. You can use KL15 if you don't need USB, or the bigger KL26 (100 or 121 pins) if you need USB and the 4 diff. inputs.

Regards,

Santiago

951 Views
ilancohen
Contributor II

Thanks for the quick response

Envoyé de mon iPhone

Le 20 oct. 2014 à 17:32, Santiago Gonzalez Fabian <admin@community.freescale.com> a écrit :

hi everybody ,im working with te kl25z microcontroller i need to do 4 differential adc ,i menaged to find 2 pair the PTE20,PTE21 and the PTE22,PTE23 but where are two more pairs i dosent find them help ???

reply from Santiago Gonzalez Fabian in Kinetis Microcontrollers - View the full discussion

Hello,

On the KL25 there are only two pairs of differential analog inputs available. You can use KL15 if you don't need USB, or the bigger KL26 (100 or 121 pins) if you need USB and the 4 diff. inputs.

Regards,

Santiago

Did your question get answered?

If so, say thanks by clicking Correct Answer in the community thread!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in Kinetis Microcontrollers by email or at Freescale Community

Following hi everybody ,im working with te kl25z microcontroller i need to do 4 differential adc ,i menaged to find 2 pair the PTE20,PTE21 and the PTE22,PTE23 but where are two more pairs i dosent find them help ??? in these streams: Inbox

0 Kudos
Reply