hardfault issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hardfault issue

1,233 次查看
pandi
Contributor III

 In mkv31f12vll12 controller using ADC inject trigger method  configure when I configure  PWM pin program stuck in HARDFAULT HANDLER  any suggestion let me know

The below line is for configuring PWM pin

PORT_SetPinMux(BOARD_FTM0_CH0_PORT, BOARD_FTM0_CH0_PIN, kPORT_MuxAlt4);

  1. Screenshot 2023-12-29 110031.pngScreenshot 2023-12-29 110031.pngScreenshot 2023-12-29 120029.pngScreenshot 2023-12-29 120029.pngScreenshot 2023-12-29 120058.pngScreenshot 2023-12-29 120058.pngScreenshot 2023-12-29 120129.pngScreenshot 2023-12-29 120129.png

 

 

 

0 项奖励
回复
2 回复数

1,195 次查看
pandi
Contributor III

if anyone know let me Hardfault issue

BR

PANDI

0 项奖励
回复

1,187 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Before you write the PORTx_PCRn reg, you have to enable the PORTx gated clock by setting the PORTx bit in SIM_SCGC5 reg.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1704250334423.pngxiangjun_rong_0-1704250334423.png

 

0 项奖励
回复